Other Parts Discussed in Thread: BQ24040
Hi
The customer is using BQ24081.
However, LED operating is different from customer specification.
LED blinks in no battery condition, I understand this is the default action.
Q1) Can I turn off the LED in the no battery state?
Q2) If LED off doesn't work, please recommend a product that turns off LED on no battery. The same specification as BQ24081 is fine.
Spec : 1 cell, charge voltage 4.2V, charge current 1A or 1.5A