Part Number: BQ25155EVM
Other Parts Discussed in Thread: BQ25155
Hi,
Condition: device in Low power Mode, VIN < VUVLO, VBAT > VBATUVLO so the battery discharge FET is turned on connecting PMID to the battery.
Event: VBAT < VBATUVLO
- After the event the system powered via PMID turns off. Correct ?
- What happens in this situation to device BQ25155 itself ?
According to what reported in the chapter 10 Power Supply Recommendations of the document bq25155.pdf,
The battery voltage must be higher than 2.4 V or VBATUVLO to ensure proper operation [of the BQ25155]
- What happens when VBATUVLO is set to 2.4 V ?
But in the description of the BUVLO Register (Address = 0x16) it is reported:

- What happens when VBATUVLO is set to 2.2 V ? According to what reported above, the device needs at least 2.4 Volts.
Thanks in advance for your kind support.
Riccardo Gaiati