Hi
Could you help check the TPS53819A schematic as below and any need to adjust
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Could you help check the TPS53819A schematic as below and any need to adjust
Thanks
Hello,
One recommendation I would have is to increase the PG pullup to 10kohm consistent with the recommendation in our datasheet:
I am assuming the PMBus pins are pulled up appropriately with whichever source is driving the communication. If that is the case, no changes need to be made there.
As far as the output capacitance and inductor selection goes, what is the intended switching frequency for each device? Do you plan to use the 425kHz default?
Regards,
Alec Biesterfeld
Hi Alec
Thank you very much
I want to know two configuration:
1, If we plan to use the default switch frequency 425K HZ, how to change the output capacitance and inductor?
2, If we plan to use the components of this circuit, how to set the frequency?
Hi Gareth,
To answer your questions:
1. Section 7.4.3 of the datasheet details how to size the output capacitance in relation to switching frequency.
2. The switching frequency is programmed to NVM by default at 425kHz. You would need to program the FREQUENCY_CONFIG command in order to change this.
Regards,
Alec Biesterfeld