Other Parts Discussed in Thread: TPS23750, TL431, , TPS23730, TPS23731, TPS23734, TPS23753A, TPS23755
I have this part designed in, it's working properly, we've built 20 boards with it, but it is now not available.
I need 25 pieces in the next month for product validation. This would carry me through the end of the year, but I'm not having luck even getting a few samples. Very frustrating.
So I need to very quickly redesign using a more available IC.
I've looked at the TPS23750, '730, '734 and they all should be able to do the job, but none of the suggested circuits or EVM topology meet my need.
I only need to supply 10Watts. I already have a transformer and would like to keep using it. The TPS23758 design uses Flyback topology and Primary Side Regulation. My regulation needs aren't super stringent. I want to keep the Flyback topology. PSR would be nice but I can add a TL431 and optocoupler if needed. According to the datasheets, all the parts I've been looking at can to Flyback and PSR.
The biggest problem is that this redesign must work the first time and none of the eval / suggested circuits I see are close enough to give me confidence they will work first time.
The 23758 worked perfectly the first time. I'm not new to SMPS design / layout, so this is not a big jump for me, but I want to have a conversation with someone who really knows these parts before I commit. Also if there are other ICs I should consider, I'm game.
Thanks