Other Parts Discussed in Thread: TPS54218
The datasheet section : 9.2.1.2.3 Input and Output Capacitor Selection states... "The output capacitor value can range from 10 µF up to 47 µF". Does this value refer to the capactitor placed close to the output pins on the device, or the total capacitance on the voltage rail across the whole PCB? I intend to use this device to power FPGA power rails, and generally most FPGA power rails require more the 47uF of capacitance.