I do have a LM25088 design that is to run on VIN = 26V, VOUT=24V, I_MAX=10A. The controller works excellent when the load is fine. However my spec requires my design to run at no load. So I already added some base load using resistors. If load is reduced too much, output of the controller becomes unstable. It looks like ist ist turning on and off repetetiveley.
In case I want to optimize this light load behavior, what is the reason for the behaviour and what are the settings I do have to look at?
cheers Andreas