Hi, team
1. can you check the circuit below to see why the OUT1 works like a load switch instead of LDO?
2. OUT1 works from 12V to 11.9V, will there any problem when working under this situation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, team
1. can you check the circuit below to see why the OUT1 works like a load switch instead of LDO?
2. OUT1 works from 12V to 11.9V, will there any problem when working under this situation?
Hello,
I am looking into this, I will get back to you by the end of the day tomorrow. Thanks!
Regards,
Srikanth
Hello,
Could you confirm the value of R1107 (is it ~75KOhm)? From the labelling in the diagram, it appears like you are expecting 12V at OUT1 and providing 12V at IN. Is this true? If so, and if R1107 is ~75KOhms, then the OUT1 is acting like an LDO and not as a load switch. If you are trying to drive a load current through OUT1, then you will need some additional dropout (Vin - Vout, hence slightly larger Vin) to maintain regulation of 12V at OUT1. Thanks!
Regards,
Srikanth