Part Number: TLV1117LV
Other Parts Discussed in Thread: TLV1117,
Let me ask you two questions when using the TLV1117LV33DCYR.
The first question is about the input capacitor 10uF and the output capacitor 100uF in Figure 9 of the data sheet. Considering the DC bias characteristics of the capacitors, the capacitance of the input capacitor 10uF is about 2.7uF, and the capacitance of the output capacitor 100uF is 24uF. In this case, connect four 10uF capacitors in parallel to the input section and four 100uF capacitors in parallel to the output section. Is it better to maintain 10uF in the input section and 100uF in the output section? Or is it better to connect only one 10uF capacitor to the input section and one 100uF capacitor to the output section, including the capacitance reduction due to the DC bias characteristics of the capacitor?
The second question is about startup characteristics. The datasheet does not list the startup characteristics. Could you give us some information about the characteristics of how many seconds the VO is output to the input VI?