Hi,
I'm using 30V to 5V conversion with LMZM33606.
I used SS pin connected to three different option.
Option 1: 5mSec,
Option 2: 11mSec and
Option 3: 16.5mSec.
when I select the capacitor to achieve 11mSec. I observed 8.5mSec as a SS. I measure the capacitor before assembly 22nF and after assembly it has become 17.7nF
with the formula 17.7nF = ~8.5mSec. which is matching with observed SS.
Can you please clarify
1. that are the possibility to reduce the capacitor value.
2. Do we have any internal capacitor which is reducing the capacitor value