Dear team,
My customer don't use watchdog function, so they plans to float pin 10. Is this feasible? Is there any bad impact?
Thanks & Best Regards,
Sherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
My customer don't use watchdog function, so they plans to float pin 10. Is this feasible? Is there any bad impact?
Thanks & Best Regards,
Sherry
Hello Sherry,
The best way to ensure that there is no interference from the Watchdog functionality would be to disable it by a providing a Digital high signal to Pin 11 (~WD_EN). Voltage in the range 2V<V< 5.5V applied to Pin 11, would ensure that the Watchdog is disabled and, even with pin 10 floating, there would be no impact. Thanks!
Regards,
Srikanth