Other Parts Discussed in Thread: LM317, TL431, ATL431, ATL431LI, TL431LI
Hi,
1) Can you help me understand the difference in output voltage accuracy in the TPS72325 vs TPS72301 - is the change from 2% to 3% due to the accuracy of the external feedback resistors or are there other differences in the parts that mean the TPS72301 is not as accurate? I need the 2% accuracy the TPS72325 offers but with an adjustable output. I'm hoping I can use the TPS72301 with 0.1% resistors to get close 2.5% accuracy or better.
2) Can these parts operate OK at no load? I'm using this as a reference rail.
3) What's the main contributor to inaccuracy - is it the load, line or temperature? Our load never exceeds 50mA and our temperature is up to 85C.
Many thanks