This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2931-N: Some more detail on the Reference Voltage temp co in the LM2931CMX (SOIC-8)

Part Number: LM2931-N

Hi, support team

My customer has the questions as follow:

Can you please give us some more detail on the Reference Voltage temp co in the LM2931CMX (SOIC-8)?

The datasheet specifies the reference voltage range over a much wider temperature range of -40 to 125°C and at ambient temp.
We specify a temperature range of 0 to 50 degC for our application and would like some more info so that we can determine the variation in output voltage over this range?

Conditions                                            Vmin    Vmax
IO = 10 mA, TJ = 25°C                         1.14     1.26
IO ≤ 100 mA, −40°C ≤ Tj ≤ 125°C        1.08     1.32

Thanks so much.

Best regards,
Yuki