Hi E2E Team,
We are using LM51561H as a flyback boost converter in our design. Below are operating conditions-
1) Input voltage: 18V to 32V
2) Output power: 65W (1.25A@54V)
3) Flyback Transformer: Attaching the transformer specification sheet. Please review and let us know if any modification is required.
I am attaching the schematic and BOM for the design. Please review and share your review comments.
Below are our queries:
1) Please let us know how we can estimate the input and output snubber circuit components value (R1, R2, C1 and C6) during design time.
2) As per my calculation output reflected voltage will be approximately 14V so MOSFET VDS > 32V +14V. Is our assumption correct? Also, is the calculated output reflected voltage correct? If not, please share the formula for the same.
3) Below are the specifications of selected diode (SK320A R3G):
a) Repetitive peak reverse voltage: 200V
b) Reverse voltage (RMS value): 140V
As per our understanding diode reverse voltage > 185V. Is SK320A R3G suitable for our design or we need to change it? If yes please let us know the reverse votlage of the diode.
Best Regards,
Aditya Kumar Singh
LM51561H_Boost_BOM.xlsxBoost Regulator.pdfLM51561H_Flyback_Transformer_Spec.xlsx