Other Parts Discussed in Thread: TIDA-010208
Hello,
My design is in the final stage for the release and a brief about the design is available below.
Cell configuration: 4S to 16S (Configurable)
Cell Chemistry: LFP and NMC
Operation: Standalone and Host Control
MCU is supplied with 5V and 5V IO's.
Maintained similar auxiliary power strategy used as in TIDA-010208 except LDO section.
Need clarification on below points:
- Both REG1 and REG2 configured to 5V. REG2 is to power up MCU during standby and shipping mode (Similar to TIDA-010208). Will there be any issue at low BAT voltage (10V) in 4S configuration using both regulator output as 5V?
- REG1 is configured to 5V and as per datasheet DIO's refer REG1 output.In the datasheet (7.6 Digital IO) output logic levels are specified w.r to VREG1, where as input logic levels are specified w.r to Vreg_1v8. Are these digital inputs are 1.8V logic only? Need this data to verify the compatibility with a 5V IO MCU.
- Planned to use HDQ and DCHG lines as temperature sensing lines.Will these lines refer to 1.8V supply or 5V(Vreg1 configured to 5v)?
- Whether is it possible to configure individual digital IO on AFE to any power supply or is there inter dependency on other IO's and functions?
- What would be the supply current of AFE in normal mode where RGE1=REG2=5V,CHG= ON in 11V overdrive mode, DSG = ON in 11V overdrive mode condition?
- Is it possible to configure REG1 as 5V alone and share the same supply with MCU by avoiding REG2 OFF?
- What is the maximum battery voltage used in TIDA-010208?
- What is the function of 0.1uF capacitors across the MOSFET'S in mosfet paralleling section in TIDA-010208?
- What is the purpose of reverse bias diode across Pack+ and Pack- terminals?
- Why Q29 is rated for 60V only?
Regards,
Ravi