I am using the UCC2864 in a conventional PFC converter. For my application i want to disable the burst mode, to do so i followed the advice given in an other topic to connect the BRST Pin directly to GND.
@230 VAC input the controller still enters burst mode below 50 W.
@ 120 VAC the the controller enters Burdt mode onlx below 20 W.
As referece i used the 400 W evaluation module, which enters BRST below 20 W @230 VAC.
What factors influence the threshold if the BRST pin is grounded.