Other Parts Discussed in Thread: TPS3850
Dear all,
I read multiple threads
that mentioned the TPS3305-33DGN watchdog WDI can be disabled by leaving it to float. However this defeats the purpose of using this chip because if I do not need a watchdog would have got a power management reset chip without the watchdog. If i connect the WDI to a CPU, how can I enable or disable the watchdog WDI? My understanding is that I have about 1.6s to start the waveform generator or the watchdog kicks in. With an older CPU, the init time is much slower so I will need control of the time to enable/disable watchdog, ideally to enable watchdog after our device boots up initialization.
What is the correct method or circuitry I should be considering to enable and disable watchdog of TPS3305 with control from micro?
Thanks