Hope that someone could help me with which device is best to use for the following boost circuit application.
- input voltage is +48V with ±4V tolerance.
- output voltage is 160V
- Boost current should be firmware adjustable through analog voltage and should not exceed input current of 3A or 6A (two different configurations)
- Enable / Disable of boost circuit
- Small footprint and high efficiency will be nice.
The LM5156H device can do the boost function but it does not have any current limiting control. Are there any other devices that may have a current limiting control.
Thanks,
Manie