Table 6-1 describes VNEG as "Negative supply output, bypass to ground with 2.2-µF capacitor". Figure 10-1 shows the VNEG capacitor connected to source not ground. Which is correct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Table 6-1 describes VNEG as "Negative supply output, bypass to ground with 2.2-µF capacitor". Figure 10-1 shows the VNEG capacitor connected to source not ground. Which is correct?
Also Figure 12-2 shows the VNEG cap connected to source. I'm leaning towards this being correct, but I would like clarification.
Hi Bryan, thanks for your question. We apologize for the confusion - the GND pins on the LMG3425 are internally connected to the the source. This is why the VNEG bypass capacitor on the high-side device is referenced to the SW node. We are looking at updating our data sheet to reflect these changes that were made in the second generation devices.
Best regards,
John