Hi Team,
My customer is looking for a low noise input source for their audio op-amp and their supply voltage is 3.3V, and they also wanted to maintain the output voltage as closed to 3.3V as possible to maintain the signal swing. They only need 5 ~ 10mA current.
If we use the TPS7A2033 as a pass through (input 3.3V, output also 3.3V), will the LDO be able to improve the output noise? Data sheet stated the output noise spec is tested with Vin >= Vout + 0.3V (consider 145mV dropout at 300mA output current). With 5 ~ 10mA output current, the voltage drop across the LDO will be < 5mV. Will setting the output voltage to 3.2V with 3.3V input be sufficient to keep the output noise to ~ 10uVrms?
Regards,
SK Loo