When the OLED brightness reaches 30%, the OUTPUT of LM27313 is normal, as shown in Figure 2. However, when the OLED brightness reaches 60%, the output of LM27313 is unstable, and the oscillometer shows sawtooth wave, as shown in Figure 3. Figure 4 shows the power parameters of THE OLED screen.