Customer mentioned during surge test, the VDD voltage test might be transient up to 25V for about 10S. Is it safe to use a Zener diode or TVS diode for VDD? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Customer mentioned during surge test, the VDD voltage test might be transient up to 25V for about 10S. Is it safe to use a Zener diode or TVS diode for VDD? Thank you.
10 seconds is a relatively long time. They may be able to use a TVS if it has enough power rating to survive 10s.
Several things to consider when selecting the TVS:
1) The ABS MAX of the UCC28C42 is 20V, recommended working range of UCC28C42 is 18V maximum. Some kind of clamp is necessary for 25V input.
2) TVS can have a wide range of clamp voltages, min/typ/max.
3) TVS must clamp at 20V maximum. Also, minimum clamping voltage must be above customers maximum VDD working voltage.
Regards,
Eric