This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS732-Q1: need the DCQ package information

Expert 7280 points
Part Number: TPS732-Q1
Other Parts Discussed in Thread: TPS732

Dear team,

DCQ package information and thermal metrics are nowhere to be found in the datasheet of TPS73218QDCQRQ1.

Can you share with me these details ?

Thanks a lot!

Best regards,

PA

  • Hi Pial,

    See below the thermal information for the DCQ package. I'll make a note to get this info added to the datasheet.

    Theta JA-High K 

    85.5

    Theta JC, top 

    46.6

    Theta JB 

    11.3

    Psi JT 

    4.9

    Psi JB 

    11.0
  • Hello Nick,

    Thank you very much for your help.

    Can you also help me on below:

    1. can you share the pinout of the DCQ package ?
    2. why are the DCQ thermal metrics for the -Q1 version are so far away from the industrial version ? - I was expecting fairly similar values

    Thanks again!

    Best regards,

    PA

  • Hi Pial,

    TPS732 datasheet has the pinout - I'm not sure why the -Q1 datasheet does not have it:

    As for the thermal metrics, the die attach materials used should result in the -Q1 version actually having slightly worse thermal metrics, so this leads me to believe that the difference is due to differences in the simulation setup used to get the numbers. The -Q1 version was released 2 years after the industrial version, 2003 vs. 2005, so I would suspect that there was some change in the board layout used or something similar. 

    Regards,

    Nick