Hello,
I've downloaded the TPS274160B pspice model for Orcad Pspice model.
I used it at Orcad Pspice 16.6, and it worked fine.
I tried to use it at Orcad Pspice 17.4 (meaning that I added the library at the simulation profile), and when I tried to run the simulation I got the next warning (U6 is the TPS274160B):
"WARNING(ORCAD-2445): Instance U6: SCHEMATIC1, PAGE1 (8.90, 2.90). not found in the configured libraries."
The simulation output wasn't correct (I used the same simulation setup from the 16.6 version), It showed that the output is disabled when it should be enabled.
Is there a problem at Orcad Pspice 17.4 with this pspice model?
If not, what can be the problem?
Thanks,
Asaf