Other Parts Discussed in Thread: UCC28951, UCC28950
Hi,
in our Phase-Shift-Full-Bridge DC/DC we have the issue, that the primary (HV-Current) has not the expected waveform. We tried several things to get an idea why:
First we change the external leakage inductance between 4,7uH and 22uH but it has no big impact on this behavior. This leakage inductor is currently a metal powder-torroid which is not in saturation.
Then we changed the transformer from planar (with its higher parasitic prim.C= 312pF) to a regular one with lower parasitic capacitance (16pF), but also no big impact on this behavior.
Somebody an idea where this could come from?
CH1 LV-Current (Load)
CH2 Switchnode T1/T2 (left Halfbridge)
CH3 Switchnode T3/T4 (right Halfbridge)
CH4 Primary Current (Transformer 14:1)