Other Parts Discussed in Thread: BQSTUDIO, EV2400, BQPRODUCTION-SINGLECELL
how to upload the golden image file ( gg.csv) file to bq27542 through I2C interface? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
how to upload the golden image file ( gg.csv) file to bq27542 through I2C interface? Thanks
Hello Tong,
Here is a link to the thread that discusses generation of the golden image
Hello Tong,
ok, glad you understand the golden image part. The gg.csv contains the values of data memory parameters. You can refer the TRM section that references how to write data memory to send I2C commands to write the values from the gg.csv
Hi Shirish,
gg file is convenience for changing the parameters.
Another question, For massive manufacturing test, , is there any tool (not the bqstudio) to dump the image file to the device? There are three type of image files that bqstudio will be generated and And which file should we use ( srec file, bq.fs file, df.fs) in production test.
Thanks
Hello Tong,
Have you looked at BQPRODUCTION-SINGLECELL? If you don't have an EV2300, then an alternative MKST-3P-ALT-EV2300 is available.
Hi Shirish,
I don't have EV2300, EV2400 will work? I have downloaded the BQPRODICTION-SINGLECELL application, but in the "Select Device bqz Container" drop down list , there is only one device (0320_0_10-bq27320.bqz) can be selected. my device is bq27542-G1. Thanks
Hello Tong,
EV2400 does not work. bq27542-G1 is an old device. I will need to check if BQPRODUCTION-SINGLECELL can support it.
I sent you a friend request on e2e, that will allow us to communicate privately for debug / trials if required