Other Parts Discussed in Thread: LMR16030,
Hello,
in our Design with LMR16006 and LMR16030 in a BLDC Controller almost all LMR16006 fails after some time of driving.
And sometimes the LMR16030 fails with broken case.
Both are not burned.
LMR16006 just stop working (output 5V) and sometimes following LDO's fails (max 5.5V Input)
LMR16030 has broken housing
Supply Voltage is a 8S Lipo Battery.
With a 4S battery we don't have Problems
Could the DCDC's fail because of high Voltage spikes on input?
The Input's are directly connected to the Battery, without TVS or protection
Maximum Voltage is planned for 10S = 42V
which protection could we add?
Greetings