Other Parts Discussed in Thread: LM5146,
In my LM5146 design, my high-side FET is the CSD19538Q2 which has around 0.6W of loss in the 2x2mm package. Is this too much loss for that small package to handle? Also, the thermal resistance is 65W/C, but that is under the ideal conditions stated in the datasheet. In my buck application, the high and low-side FETs will have to be close together and the overall board size will be quite small (probably around 1in2 or less). For this reason, we estimated that the thermal resistance under these conditions would be around double that of the value in the datasheet. Are there more accurate ways to estimate this, or do you have a better estimate for the temp rise in the CSD19538Q2?
Thanks,
Thomas