This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82150: TPS82150 start up time

Part Number: TPS82150

Hi

I want to ask about TPS82150's start up time.

I simulated TPS82150's start up sequence using PSpice for TI.

I made 5V,3.3V,1.8V,1.2V & 1.0V from 12V using this IC.

Start up sequence is below

 1st start up :5V,1.0V

 2nd start up:1.8V,1.2V (using PG made from 1.0V IC)

 3rd start up:3.3V(using PG made from 1.8V IC)

I noticed that start up times are different  of all voltage ICs.

Css/TR capicitor's value are 470pF in all voltage ICs.

According to the datasheet, I think that start up time will decide from Equation (7).

So I thought the time was the same for all voltages because the capacitors have the same capacitance. Can you tell me why they are different?

Best regards

Naoki