Hi,
I have a question about feedback resistor on TPS784-Q1.
I want to use the following four voltages: 3.0V, 2.8V, 1.8V, 1.2V
I calculated the resistor value through Equation 2, and I'm asking if there's any problem with using it as follows:
3.0V -> R1 : 30K, R2 : 20K
2.8V -> R1 : 20K, R2 : 15K
1.8V -> R1 : 10K, R2 : 20K
1.2V -> R1 : 0, R2 : 10K
Thank you.