This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25149-Q1EVM-2100: heavy load startup, see overshoot on current

Part Number: LM25149-Q1EVM-2100

Hi, team

when start up with heavy load(13A), see overshoot on Iout. Is it normal? and what can cause this overshoot? (such as test method?)

test condition: Vin=12V Vout=3.3V Iload=13A