Hello,
I was hoping to use a resistor and a DAC to control the output of LM2931 using a microcontroller like it was described here: https://training.ti.com/voltage-regulator-margining-precision-dacs.
I was successful using this technique with a different LDO, but this one has a different formula for Vout (Vout=Vref(1+R2/R1) instead of Vout=Vref(1+R1/R2)).
This is the schematic that I used:
The nominal output voltage was calculated at 9V and R3 was calculated for an output voltage range of 1.2V to 10V while the voltage range of the DAC is 0.2V-3.1V.
I can measure an output voltage of 8.96V while the DAC is not connected, 1.49V for a DAC output of 0.2V and 4.54V for a DAC output of 3.1V.
These are the measured output voltage levels with different R3 values:
R3 | 56K2 | 9K09 | 4K22 |
Output at 0.2V | 3.27V | 1.53V | 1.37V |
Output at 3.1V | 5.48V | 4.57V | 4.45V |
Is there a different configuration that I might try in order to get the full desired output voltage range of 1.2V to 10.0V?
Thank you,
Alex Chitic