Other Parts Discussed in Thread: LM3553, TPS92200, LM3405, TPS61165
Hi TI :
I use LM3553,and the Vf of LED is 3.3V, the current
For the input is 5V,I measure the output voltage is 5V.
If I change the input voltage to 5.5V,the output can still be 5V ?
LM3553 is boost LED driver.
I am afraid of the output can not be 5V.
Or the output voltage will be 5.5V
best regards