Dear Support team,
I have some question regarding Figure 10-25 in datasheet p.29 below.
Could you please support it?
Q1. What does the 85V rectifier diode on D2 do?
Q2. Voltage is detected by a voltage divider resistor directly from the input side to the OV terminal without using VSNS and SW.
Why not use SW? Is the VSNS connected to the Cvs via 10k Ω to avoid voltage delay? Is there any other reason?
Q3. What is the role of CCAP?
Q4. What is the reason for the D3 and D4 combination? If you put in D3, does it not have to be bidirectional with D4?
What are the benefits of this combination?
Best Regards,
Hirokazu Takahashi