Hello,
Currently the VLDO2 is connected to SYS (VINLDO) through a 0ohm resistors, no cap. VLDO2 is not being used in the design and was disabled.
When the PMIC goes to sleep, it is pulling ~10mA from the battery. No power source on the AC and USB. Removing the 0ohm resistor, leaving VLDO2 floating, the sleep current is much lower, <1mA.
Can VLDO2 be left floating in the final design?
Thank you