Hello,
monitoring continously the state of charge, this is not updating correctly.
In particular, when I reboot the entire custum board, the values are updated differently from the previous reading.
I will give you an example.
I turn on the board and the state of charge is 80%. After 5 minites it changes to 79%.
Then, I reboot the board and the new state of charge become 75%.
The component is not in hibernate mode.
How can I get rid of it and monitor correctly and continously the state of charge?
Thank you