Hi,
I have some queries with regards to current monitor pin settings on LM73100 & hope to get some clarification on it.
1. In the LM73100 datasheet, it is strongly requested to ground the Imon pin if not used. Is there any specific reason for this? I did look into datasheet section 7.3.5 for answers but I'm still unsure reason for this design recommendation.
2. Also I did encounter similar issue on eFuse application as well where there was no clear definition of Imon pin setup, will it be the same recommendation applied onto LM73100 as well?
3. What is the backward leakage current at Vout=10V if the IC input is open (OVLO= 0V)?