This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z60EVM-578: Learning Cycle Failure

Part Number: BQ40Z60EVM-578
Other Parts Discussed in Thread: BQ40Z60

Hello,

I've been working with the BQ40z60 for about a week and I'm having trouble with completing a learning cycle and getting an accurate SoC reading. I've used the GPC tool to get a chem ID for my battery but I believe that my settings are still off. I have attached a short log of my battery at rest, along with the data memory register file and the GPC log. 

Battery Information:

Battery Manufacturer- Turnigy

Nominal Capacity- 460mAh

Nominal Voltage- 7.4V

Cell Count: 2

Chem ID used: 1372

Wed Aug 25 15:27:31 PDT 2021

Device Version Info = 4600_0_15
BQZ Device Name = bq40z60
BQZ Firmware Version = V0_15_BLD21

Design Capacity = 460
Design Voltage = 7400
Specification Info = 0x0031
Manufacturer Date = 1980-1-1
Serial Number = 0x0001
Manufacturer Name = Texas Instruments
Device Name = bq40z60
Device Chemistry = LION

Sample,DateTime,ElapsedTime,Temperature,Voltage,Current,LogRowTime(ms),LogStatus
1,2021-08-25 15:27:36,4.002,24.2,6019,0,40,SUCCESS
2,2021-08-25 15:27:40,8.014,0x69C1,300,10,0,65535,65535,1,24.2,6019,0,0,100,0,0,0,444,65535,65535,65535,0,0,4,-1260,-2070,100,3022,2996,0,0,6021,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,1284,16384,16384,604,SUCCESS
3,2021-08-25 15:27:44,12.015,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6019,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3023,2996,0,0,6020,12824,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1289,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1022,SUCCESS
4,2021-08-25 15:27:48,16.020,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6019,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3023,2996,0,0,6020,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1293,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1097,SUCCESS
5,2021-08-25 15:27:52,20.033,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6019,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3023,2996,0,0,6021,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1297,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1115,SUCCESS
6,2021-08-25 15:27:56,24.045,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6018,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2996,0,0,6020,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,23.9,24.0,24.2,24.2,23.9,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1301,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1039,SUCCESS
7,2021-08-25 15:28:00,28.056,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6018,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2996,0,0,6020,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1305,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1045,SUCCESS
8,2021-08-25 15:28:04,32.056,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6018,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2996,0,0,6020,12824,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1309,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1029,SUCCESS
9,2021-08-25 15:28:08,36.067,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6018,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6020,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1313,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1110,SUCCESS
10,2021-08-25 15:28:12,40.073,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6018,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2996,0,0,6020,12824,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1317,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1073,SUCCESS
11,2021-08-25 15:28:16,44.079,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6018,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6020,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1321,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1147,SUCCESS
12,2021-08-25 15:28:20,48.094,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6018,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6020,12828,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1325,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1038,SUCCESS
13,2021-08-25 15:28:24,52.097,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6018,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6020,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1329,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1112,SUCCESS
14,2021-08-25 15:28:28,56.102,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6018,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6020,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1333,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1060,SUCCESS
15,2021-08-25 15:28:32,60.115,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6017,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6020,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1337,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1063,SUCCESS
16,2021-08-25 15:28:36,64.116,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6017,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6018,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,23.9,24.0,24.2,24.2,23.9,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1341,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1108,SUCCESS
17,2021-08-25 15:28:40,68.131,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6017,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6017,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1345,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1031,SUCCESS
18,2021-08-25 15:28:44,72.143,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6017,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6018,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1349,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1036,SUCCESS
19,2021-08-25 15:28:48,76.156,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6017,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6017,12825,0,0,0,0,0,0,0,0,0,0,20.5,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1353,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1022,SUCCESS
20,2021-08-25 15:28:52,80.169,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6017,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6017,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.0,23.9,24.0,24.2,24.2,23.9,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1357,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1057,SUCCESS
21,2021-08-25 15:28:56,84.170,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6019,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1361,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1055,SUCCESS
22,2021-08-25 15:29:00,88.185,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3023,2995,0,0,6019,12827,0,0,0,0,0,0,0,0,0,0,20.5,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1365,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1055,SUCCESS
23,2021-08-25 15:29:04,92.194,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3023,2995,0,0,6018,12828,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1369,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1031,SUCCESS
24,2021-08-25 15:29:08,96.198,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6019,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1373,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1105,SUCCESS
25,2021-08-25 15:29:12,100.209,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6019,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1377,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1032,SUCCESS
26,2021-08-25 15:29:16,104.219,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6020,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1381,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1068,SUCCESS
27,2021-08-25 15:29:20,108.244,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6019,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1385,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1074,SUCCESS
28,2021-08-25 15:29:24,112.247,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6018,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1389,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1103,SUCCESS
29,2021-08-25 15:29:28,116.252,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6018,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1393,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1051,SUCCESS
30,2021-08-25 15:29:32,120.266,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2994,0,0,6017,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1397,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1132,SUCCESS
31,2021-08-25 15:29:36,124.281,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2995,0,0,6017,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1401,16384,16384,0,0,0,0,6,496,440,0,0,460,460,460,460,16384,16384,0,0,0,9,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1053,SUCCESS
32,2021-08-25 15:29:40,128.296,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6016,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2994,0,0,6017,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1405,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1023,SUCCESS
33,2021-08-25 15:29:44,132.301,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6015,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2994,0,0,6017,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1409,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1081,SUCCESS
34,2021-08-25 15:29:48,136.302,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6015,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2994,0,0,6017,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1413,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1077,SUCCESS
35,2021-08-25 15:29:52,140.316,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6015,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3021,2994,0,0,6017,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1417,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1080,SUCCESS
36,2021-08-25 15:29:56,144.321,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6015,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2994,0,0,6017,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1421,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1061,SUCCESS
37,2021-08-25 15:30:00,148.323,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6015,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3022,2994,0,0,6018,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1425,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1027,SUCCESS
38,2021-08-25 15:30:04,152.332,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6015,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3021,2994,0,0,6017,12828,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1429,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1051,SUCCESS
39,2021-08-25 15:30:08,156.344,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6015,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0010,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3021,2994,0,0,6018,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1433,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1084,SUCCESS
40,2021-08-25 15:30:12,160.357,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6015,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3021,2994,0,0,6018,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1437,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1056,SUCCESS
41,2021-08-25 15:30:16,164.365,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6014,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0004,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3021,2994,0,0,6017,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.0,23.9,24.0,24.3,24.3,23.9,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1441,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1078,SUCCESS
42,2021-08-25 15:30:20,168.376,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6015,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0004,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3021,2994,0,0,6017,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1445,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1004,SUCCESS
43,2021-08-25 15:30:24,172.377,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6014,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3021,2994,0,0,6017,12828,0,0,0,0,0,0,0,0,0,0,20.6,24.0,23.9,24.0,24.3,24.3,23.9,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1449,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1098,SUCCESS
44,2021-08-25 15:30:28,176.390,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6014,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3021,2994,0,0,6016,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1453,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1039,SUCCESS
45,2021-08-25 15:30:32,180.399,0x69C1,300,10,0x6081,0,65535,65535,1,24.4,6014,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3021,2994,0,0,6017,12824,0,0,0,0,0,0,0,0,0,0,20.6,24.3,24.2,24.2,24.4,24.4,24.2,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1457,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1107,SUCCESS
46,2021-08-25 15:30:36,184.407,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6014,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2994,0,0,6016,12824,0,0,0,0,0,0,0,0,0,0,20.6,24.2,24.1,24.2,24.3,24.3,24.1,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1461,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1068,SUCCESS
47,2021-08-25 15:30:40,188.419,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6014,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2994,0,0,6015,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.2,24.0,24.1,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1465,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1057,SUCCESS
48,2021-08-25 15:30:44,192.419,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6014,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3021,2993,0,0,6016,12824,0,0,0,0,0,0,0,0,0,0,20.6,24.2,24.0,24.1,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1469,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1057,SUCCESS
49,2021-08-25 15:30:48,196.431,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6014,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6016,12828,0,0,0,0,0,0,0,0,0,0,20.6,24.2,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1473,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1075,SUCCESS
50,2021-08-25 15:30:52,200.440,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6014,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6016,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.2,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1477,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1097,SUCCESS
51,2021-08-25 15:30:56,204.442,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6014,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6017,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.2,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1481,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1096,SUCCESS
52,2021-08-25 15:31:00,208.447,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6015,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1485,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1013,SUCCESS
53,2021-08-25 15:31:04,212.453,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6015,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1489,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1038,SUCCESS
54,2021-08-25 15:31:08,216.464,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6015,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.2,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1493,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1058,SUCCESS
55,2021-08-25 15:31:12,220.465,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6015,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1497,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1057,SUCCESS
56,2021-08-25 15:31:16,224.476,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6014,12824,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1501,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1079,SUCCESS
57,2021-08-25 15:31:20,228.490,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6014,12823,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1505,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1032,SUCCESS
58,2021-08-25 15:31:24,232.500,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6015,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1509,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1101,SUCCESS
59,2021-08-25 15:31:28,236.513,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6014,12828,0,0,0,0,0,0,0,0,0,0,20.6,24.2,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1513,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1010,SUCCESS
60,2021-08-25 15:31:32,240.527,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6014,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.2,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1517,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1012,SUCCESS
61,2021-08-25 15:31:36,244.529,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6015,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1521,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1056,SUCCESS
62,2021-08-25 15:31:40,248.533,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6014,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1525,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1036,SUCCESS
63,2021-08-25 15:31:44,252.537,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6014,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.2,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1530,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1093,SUCCESS
64,2021-08-25 15:31:48,256.551,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6013,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1534,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1064,SUCCESS
65,2021-08-25 15:31:52,260.566,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2993,0,0,6014,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1538,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1111,SUCCESS
66,2021-08-25 15:31:56,264.580,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2992,0,0,6013,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1542,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1036,SUCCESS
67,2021-08-25 15:32:00,268.581,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6013,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2992,0,0,6013,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.3,24.3,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1546,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1050,SUCCESS
68,2021-08-25 15:32:04,272.585,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2992,0,0,6013,12828,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1550,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1140,SUCCESS
69,2021-08-25 15:32:08,276.600,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2992,0,0,6012,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1554,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1047,SUCCESS
70,2021-08-25 15:32:12,280.607,0x69C1,300,10,0x6081,0,65535,65535,1,24.3,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2992,0,0,6012,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1558,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1025,SUCCESS
71,2021-08-25 15:32:16,284.620,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2992,0,0,6012,12825,0,0,0,0,0,0,0,0,0,0,20.5,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1562,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1042,SUCCESS
72,2021-08-25 15:32:20,288.632,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6012,12824,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1566,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1061,SUCCESS
73,2021-08-25 15:32:24,292.648,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6013,12828,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1570,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1093,SUCCESS
74,2021-08-25 15:32:28,296.656,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3020,2992,0,0,6013,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1574,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1070,SUCCESS
75,2021-08-25 15:32:32,300.657,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6011,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1578,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1068,SUCCESS
76,2021-08-25 15:32:36,304.671,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6011,12828,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1582,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1101,SUCCESS
77,2021-08-25 15:32:40,308.675,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6011,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1586,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1097,SUCCESS
78,2021-08-25 15:32:44,312.686,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6012,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6012,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1590,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1022,SUCCESS
79,2021-08-25 15:32:48,316.692,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6011,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6012,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1594,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1095,SUCCESS
80,2021-08-25 15:32:52,320.701,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6014,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1598,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1071,SUCCESS
81,2021-08-25 15:32:56,324.715,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6013,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1602,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1026,SUCCESS
82,2021-08-25 15:33:00,328.726,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6013,12828,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1606,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1093,SUCCESS
83,2021-08-25 15:33:04,332.727,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6014,12827,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1610,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1029,SUCCESS
84,2021-08-25 15:33:08,336.741,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6013,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1614,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1063,SUCCESS
85,2021-08-25 15:33:12,340.756,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6012,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1618,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1079,SUCCESS
86,2021-08-25 15:33:16,344.758,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2992,0,0,6012,12823,0,0,0,0,0,0,0,0,0,0,20.5,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1622,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1060,SUCCESS
87,2021-08-25 15:33:20,348.770,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6012,12824,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1626,16384,16384,0,0,0,0,7,496,440,0,0,460,460,460,460,16384,16384,0,0,0,10,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1049,SUCCESS
88,2021-08-25 15:33:24,352.785,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3018,2992,0,0,6012,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1630,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1049,SUCCESS
89,2021-08-25 15:33:28,356.798,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3018,2991,0,0,6012,12825,0,0,0,0,0,0,0,0,0,0,20.5,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1634,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1100,SUCCESS
90,2021-08-25 15:33:32,360.804,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6010,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3018,2991,0,0,6011,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1638,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1046,SUCCESS
91,2021-08-25 15:33:36,364.808,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6009,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6011,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1642,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1089,SUCCESS
92,2021-08-25 15:33:40,368.815,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6009,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3018,2991,0,0,6009,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1646,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1052,SUCCESS
93,2021-08-25 15:33:44,372.818,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6009,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6012,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1650,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1046,SUCCESS
94,2021-08-25 15:33:48,376.826,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6009,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6012,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1654,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1056,SUCCESS
95,2021-08-25 15:33:52,380.835,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6009,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6012,12822,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1658,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1125,SUCCESS
96,2021-08-25 15:33:56,384.848,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6009,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6011,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1662,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1065,SUCCESS
97,2021-08-25 15:34:00,388.849,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6009,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6011,12829,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1666,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1080,SUCCESS
98,2021-08-25 15:34:04,392.856,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6009,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6011,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1670,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1057,SUCCESS
99,2021-08-25 15:34:08,396.859,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6009,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6012,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1674,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1022,SUCCESS
100,2021-08-25 15:34:12,400.874,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6008,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6011,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1678,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1117,SUCCESS
101,2021-08-25 15:34:16,404.885,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6008,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6009,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.1,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1682,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1044,SUCCESS
102,2021-08-25 15:34:20,408.887,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6008,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6009,12825,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1686,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1025,SUCCESS
103,2021-08-25 15:34:24,412.888,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6008,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3019,2991,0,0,6009,12826,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1690,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1042,SUCCESS
104,2021-08-25 15:34:28,416.893,0x69C1,300,10,0x6081,0,65535,65535,1,24.2,6008,0,0,100,0,0,0,444,65535,65535,65535,0,0,0x02D0,4,-1260,-2070,100,0x69C1,0x0000,0x08,0x0002,0x0000,0xC5,0x000C,0x0000,0x0000,0x4001,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,3018,2991,0,0,6009,12824,0,0,0,0,0,0,0,0,0,0,20.6,24.0,24.0,24.0,24.2,24.2,24.0,-2,-1,444,340,-2,-1,446,342,444,340,24.2,24.1,1000,1000,0,0,90,127,0,0,14,0,0,0,0,0,1694,16384,16384,0,0,0,0,8,496,440,0,0,460,460,460,460,16384,16384,0,0,0,11,1.0,1000,16384,16384,0,0,0,0,0,0,0,0,0,0,0,459,353,0,0,1066,SUCCESS


bq40z60_settings.gg.csv

Chemistry ID selection tool, rev=2.52		
		
Configuration used in present fit:		
ProcessingType=2		
NumCellSeries=2		
ElapsedTimeColumn=2		
TemperatureColumn=3		
VoltageColumn=4		
CurrentColumn=5		
		
Best chemical ID : 1372	Best chemical ID max. deviation, % : 0.89	
		
		
		
Summary of all IDs with max. DOD deviation below 3%		
		
Chem ID	max DOD error, %	Max R deviation, ratio
1372	0.89	0.12
1344	1.17	0.14
1345	1.18	0.13
1375	1.19	0.14
1327	1.27	0.19
1374	1.28	0.07
1373	1.38	0.08
1452	1.47	0.2
1304	1.54	2.57
1531	1.61	0.09
120	1.63	0.35
1356	1.64	0.26
1497	1.67	0.97
1378	1.69	0.98
1371	1.75	0.97
1619	1.78	1
467	1.8	2
2116	1.8	2
2304	1.83	1.06
1377	1.83	0.98
1450	1.83	0.98
3547	1.83	1.55
1763	1.85	0.95
189	1.87	1.58
1112	1.87	0.96
1359	1.9	0.98
1376	1.92	1.26
2118	1.93	0.91
469	1.93	0.91
167	1.93	1.58
1288	1.94	1.73
1535	1.98	2.33
2195	2.04	0.81
1287	2.06	0.42
1362	2.07	0.04
1296	2.08	1.28
116	2.09	0.31
3771	2.11	1.73
1328	2.11	0.84
2290	2.15	0.76
148	2.18	0.32
1529	2.2	0.97
144	2.21	0.6
3731	2.22	1.68
1360	2.3	2.31
2892	2.36	0.23
1536	2.36	0.82
2105	2.36	1.55
1347	2.42	0.72
1530	2.43	0.99
182	2.44	0.62
2596	2.45	1.82
107	2.52	0.98
1260	2.53	2.26
533	2.54	1.56
2489	2.56	0.77
1189	2.58	2.05
1620	2.58	2.74
1751	2.66	1.13
584	2.66	0.92
2992	2.7	1
1938	2.72	2.05
1228	2.75	1.98
180	2.81	0.48
1116	2.84	0.71
133	2.86	0.43
1496	2.9	0.71
1503	2.9	0.71
1182	2.92	0.59
1188	2.93	1.96
2032	2.97	1.72
125	2.98	0.97
		
Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.		
		
		
Selection of best generic ID for ROM based devices like bq274xx		
		
		
Device / Family #1		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
354	bq27411-G1C: 4.35V LiCoO2	2.55
128	bq27421-G1A: 4.2V LiCoO2	3.18
3142	bq27421-G1D: 4.4V LiCoO2	4.16
312	bq27421-G1B: 4.3V LiCoO2	5.11
Best generic ID 354		
Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.		
		
		
Device / Family #2		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
354	bq27621:  (ALT_CHEM2) 4.35V LiCoO2	2.55
1210	bq27621:  (ALT_CHEM1) 4.3V LiCoO2	3.39
1202	bq27621: (default) 4.2V LiCoO2	3.83
Best generic ID 354		
Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.		
		
		
Device / Family #3		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
3230	bq27426: (default) 4.35V LiCoO2	3.14
1202	bq27426: (ALT_CHEM1) 4.2V LiCoO2	3.83
3142	bq27426: (ALT-CHEM2) 4.4V LiCoO2	4.16
Best generic ID 3230		
Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.		
		
		
Warning: Discharge rate is too high. High rate reduces ID detection accuracy	 10 hr rate is recomeended. Total discharge time is less than 5 hrs	 t_hrs=  3.55050833333333