Hi Team,
My customer is considering UA78L05AI now. He has following questions. Please kindly help. Thanks.
1. What is absolute maximum rating of Input voltage? Is it 30V?
2. What is Recommended Operating Conditions of Input voltage? Is it between 7V~20V?
3. What does following parameter mean?
Output voltage regulation : Does it mean voltage deviation from required value? For example, if this parameter is 60mV and output is 5V, real value may be 5V±60mV?
Output noise voltage : What does it mean and what does this affect?
Dropout voltage : Does it mean the min voltage between Vin and Vout needed to use this LDO? For example, Vin have to be 1.7V bigger than Vout in this case?
Thanks.
Regards,
Jo