Hi,
Greetings
We are using the LED Driver TLC59116 in our product for directly driving the RGB LEDs using PWM. The LEDs are driven by 12V rail and with current of around 100mA. The Heat pad of this LED driver is heating the PCB too much. And now we want to drive the LEDs with 200mA for higher intensity
So I was wondering if can we drive the LEDs using the mosfets and the mosfets through the TLC59116 output pins using PWM. Is it possible? Please let me know what I need to do to drive mosfet through TLC59116 output pins. Do I need to connect a Pull-up at the output pin of this LED Driver? Are the TLC59116 output pins capable of driving the mosfets using the PWM?
Our company had procured lot many quantities of this TLC59116 chip for production which we do not want to replace or change with other chip ?
Your help will be highly appreciated.
Please reply
Regards,
Vihang Waze
TATA ELXSI I Engineering Creativity