This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC5350-Q1: Is "IN-" pin used such as "DISABLE" input pin?

Part Number: UCC5350-Q1
Other Parts Discussed in Thread: UCC21320-Q1

Hi team, 

Is "IN-" pin used such as "DISABLE" input pin? 
Table 4. Function Table looks IN-=DISABLE(driver output=L with high level input), which is the same function with UCC21320-Q1 DISABLE pin, is it correct? 

Regards,
Ochi