Part Number: UCC28634
Hi , I am using UCC28634DR on a PCB Design for a fly back converter, designed by WEBENCH Power designer. After the fabrication and assemble of the pcb, when power was applied to the input of the circuit, the circuit did not output any voltage at all. The transformer was built using base WEBENCH specifications. What we found was the VDD pin pulsing from 5.2 to 10.1 volts over and over as well as HV pin pulsing as well. The SD pin is LOW at .145mv, it seems the circuit is in fault mode but what causing it?