Hello,
I wanted to activate pre-discharge on my BMS chip, with only timer based activation. First I thought, even if it does not activate whenever a load is connected (because DSG is already ON in relax mode), it should has no harm to have pre-discharge. it some scenarios it can help, such as automatic recovery from OCDs, where DSG is turn off and on.
However, there is something that concern me. DSG is also used in high-ampere charging. activating PDSG in that case, not only is meaningless, but can also be harmful. When the charge current suddenly rises, if DSG does not turn on quickly, the body diode can be damaged. If first PDSG turns on, still DSG's body diode is active.
Then, shortly, PDSG should only be activated when DSG is going to be turn on for discharging, not charging. it is like that?
thanks