The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS566231: TPS566231PRQFR

Part Number: TPS566231
Other Parts Discussed in Thread: TPSM82823, TPS62865

Hi, 

We are using TPS566231 on our custom board to generate a 5V with up to 4.5A current. this 5.0V buck feed other DC-DC convertors likeTPS62865 and TPSM82823 to generate more voltages.

Looking on table 8-2 in the datasheet, I see 220uF is the maximum Cout you are recommended, is this the maximum value we can use for 5.0V customers including caps on TPS62865 and TPSM82823?

And what is the max Cout of TPS62865 and TPSM82823 ?

Thanks,