Hello Guys,
Good day.
Our customer wanted some clarifications on TPS92515 dimming ratio: There is a dimming range sited on the first page of the TPS92515 datasheet for each of the three methods: 10,000:1 for Shunt PWM, 1,000:1 PWM, and 200:1 Analog. In Section 8.3.11 an example is given that for (Series) PWM the dimming range reduces from 1,000:1 to 500:1 at 10kHz, because of the 200ns minimum gate delay + slew time. That, the customer understand. What he do not understand, and would like to understand, is how to similarly estimate the Shunt PWM dimming range (through theory not simulation).
He understand the external FET could be a limiting factor, but assuming that is well chosen, what about the TPS92515 limits the dimming range? For example 10,000:1 has been chosen, how was that calculated?
Thanks and regards,
Art