This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM43601-Q1: OUTPUT IS NOT GENERATED AUTOMATICALLY

Part Number: LM43601-Q1
Other Parts Discussed in Thread: LM43601

lm43601_12V_SCH.pdf

PFA the Schematics

Input Voltage => +12V

Output Voltage => -12V

Pls. note as of now we have not assembled J7 Common Mode Inductor.

At first POWER ON the output is disabled i.e we don't get any output but after removing and reinserting only the JP5 Berg the IC starts giving the desired output.

After that if we POWER ON and OFF the input voltage within sometime then each time the IC gives the output automatically.

If Power On after approx 3 mins or later then again we don't get the output, again we need to remove and reinsert the JP5 Berg to get the output.

The same phenomena is observed in the both the pcb's that we have assembled so far.

Pls. let us know how to ensure that the IC gives the output automatically without manual intervention (removing and reinserting the JP5 Berg).

Thanks and Regards

Ravi Chawda