Other Parts Discussed in Thread: UCC28740, UC2843
Hi
I need to design DC DC converter using UC2843A having input voltage 40 - 60VDC and variable output 10A current limit. This will be used to charge the Li ion battery having BMS in place with switching in -ve line. BMS can charge the battery with 50A current if the current is >50A, DC DC converter will take over and charge the battery with constant 10A. Battery +ve is directly connected with charger and in the -ve line MOSFETS are placed as switch. Please suggest how to achieve the DC DC converter design.
Thanks
Sandeep