Other Parts Discussed in Thread: TPS2116, TPS2113A, TPS2115A
Hi Team,
I am using LM66100 in one of my projects.
In the datasheet of LM66100, it says we can use two of such chips to OR the input voltages and let only one of the input with higher potential to the output.
How it can be implemented?.
The only chance I see is to connect the ~CE pin of one of the LM66100 to the VIN of the other diode and vice versa. If this needs to be working, the VIN pin should be actively pulled down to 0V.
Is my understanding is correct?.
Also, if I need to disable the ideal diode, the only way is to pull the CE pin above VIN with a minimum of 80mV, what should I do if Vin is the only power source in my system?