This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146-Q1: About the hysteresis set of LM5146

Part Number: LM5146-Q1
Other Parts Discussed in Thread: LM5146

Hello

I'm in a trouble about the hysteresis set of LM5146 .please help me and give me some suggests ,thanks

if I want to use the GIPO enable the LM5146 or use a IGN to enable the LM5146 ,Theoretically,  should my gipo output  be connected behind the comparator??? But I can't do it according to the current structure  .The picture shows that it is connected between two resistors ,so EN/UVLO will be 3.3V when GPIO is 3.3V , right?

1.