Other Parts Discussed in Thread: LM5146
Hello
I'm in a trouble about the hysteresis set of LM5146 .please help me and give me some suggests ,thanks
if I want to use the GIPO enable the LM5146 or use a IGN to enable the LM5146 ,Theoretically, should my gipo output be connected behind the comparator??? But I can't do it according to the current structure .The picture shows that it is connected between two resistors ,so EN/UVLO will be 3.3V when GPIO is 3.3V , right?
1.