This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79606EVM-897: wrong balancing

Part Number: BQ79606EVM-897
Other Parts Discussed in Thread: BQSTUDIO

hi,

we are testing the EVM and something seems off on the cell voltage monitoring, when testing the balancing.

I have connected a battery stack with 6 cells on pins 2 to 8 an left Pin 1 & 9 Unconnected.

I have jumper J2 and J3 ON to power the board from the battery

I have the SW2 on the OFF position and the on-board resistor ladder is Unconnected

BQstudio SET UP

I have the following configuration for Cell Voltage monitoring and Balancing

When I enable Balancing without the comparator the CB_RUN is completed

Then I check the Cell voltages during the balancing procedure.

The cell that is “bleeding” current has a voltage drop when measuring, around 0,665 Volts, and the cells that are next to the “bleeding” cells have a voltage rise.

 

ODDS balancing

EVENS balancing

Also because of the Voltage measurements are like this if I activate the Comparator, it immediately “completes” the balancing (I guess because CB_DONE_THRESH is triggered and CB_DONE is then set).

What are we doing wrong?

thansk a lot in advance

KR

Vincenzo